This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC Data Acquisition rate on OMAPL138

Other Parts Discussed in Thread: OMAPL138

Hi Sir/Madam,

1)  In our project we are using Few  environmental  sensors like Gas , Temperature and Humidity Sensors  to acquire analog data which operates below 20khz range, But the ADC chip available on the Logic PD EVMOMAPL138 board   has ADS901E which operates in the range of  73.2421875KHz to 1.171875MHz.
       So kindly suggest the steps need to be followed to acquire the data  below 20Khz range.
2) In ADS901E Chip the capacitor (0.1uf) is connected in series to pin no 27 as an Analog input but the problem is the capacitor which is connected in series will block the  voltage and doesn't allow the Signal to pass through.
        So Kindly suggest the ADC compatible with OMAPL138 that is capable of handling data below 20Khz.