Other Parts Discussed in Thread: ADS131E08EVM-PDK, ADS131E08
Can anybody give more information on the MMB0 motherboard? All I can find is the schematic.
I am working with the ADS131E08 in a power meter application. The ADS131E08EVM-PDK user's guide states that the ADS131E08EVM comes with a motherboard, MMB0, and appears to be ready to interface with a PC right out of the box. The only information I've been able to find on the MMB0 is the schematic, from which I can see that the DSP on the board is the TMS320VC5509APGE. Will I be able to program this DSP on the MMB0 in the same manner that it would be programmed if I were using the TMDSDSK5509A DSK or the C5502 eZdsp Development Kit?
ADS131E08EVM-PDK user's guide: http://www.ti.com/lit/ug/sbau200/sbau200.pdf
C5502 eZdsp Development Kit: http://www.ti.com/tool/tmdx5509ezdsp
TMDSDSK5509A DSK: http://www.ti.com/tool/tmdsdsk5509