Other Parts Discussed in Thread: LM95213, LM84, LM95233
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LM95213, LM84, LM95233
Hi Ryuji
There aren't any application notes related to the thermal diode in the LM97600.
We highly recommend using a remote diode temperature sensor IC like the LM95213. This type of device uses readings at 2 different current levels to provide a relatively accurate measure of the die tempeature.
Other methods will work, but will usually require the user to perform calibrations to get an accurate measurement.
I hope this is helpful.
Best regards,
Jim B
Hi Asaka-san
For reference, here is the information listed in the datasheet:
The measurement is done by applying a DC current through the thermal diode. Two different currents are applied (12uA and 192uA). The voltage at each current is measured, and the difference between the voltages is determined. This measurement is done at junction temperatures of 25 degrees C and 85 degrees C.
I hope this is helpful.
Best regards,
Jim B
Hi Asaka-san
The dual current method is similar to that used inside the remote diode temperature sensing ICs like the LM95233 and similar devices. Even though the current magnitudes may be different this type of sensor IC will provide a relatively accurate measurement of the LM97600 junction temperature.
I hope this is helpful.
Best regards,
Jim B