Hello,
I'm trying to do some basic calculations regarding the common mode and differential inputs for the ADS1x48 device.
May I ask:
If my Pt100 sensor recommends a max current of 1mA and I use it in 3-wire mode, does this mean the maximum I can put through each limb is 500uA (total through Rbias = 1mA), or 1mA (total through Rbias = 2mA)?
What voltage am I aiming to get across Rbias? AVDD/2 or 2.048V? I'm using a 3.3V supply, so AVDD/2 = 1.65V
Can you also help me work through an example:
If I have PGA=128, this will give me a max differential input of 12.9mV. If I have Rcomp = 100ohms and I want to measure a Pt100 RTD at 37C = 114.4ohms, I'm really trying to measure 14.4ohms.
So for example with 2x500uA IDACs (refers to my question regarding how much current is passing through the RTD), my max diff input will be on the order of 2.2mV (0.5mA*14.4ohms), giving me plenty of headroom for this PGA setting. My modulator voltage will then be 128*2.2mV=280mV.
How do I then relate these numbers to choosing an Rbias value to get to the middle of the common mode voltage for my inputs (relating to my questions regarding the desired Vref)? In a 3-wire setting, do I use Vref_desired/(2*IDAC)?
Many thanks!
-Rob.