Other Parts Discussed in Thread: TVP7002
Hi Sirs,
I have captured VGA input source via TVP7002.
I could distinguish what input resolution is and set the TVP7002 registers.
Everything seems OK but the captured video has horizontal-shaking at some VESA standard input.
After modifing H-PLL Phase Select register(0x04h in tvp7002),
For example 1080P60 VGA input,
I modified H-PLL Phase select register from 0x80 to 0x00 (180 degrees to 0 degrees)
The horizontal-shaking has improved!!
BTW, how to adjust the Phase select setting properly? any rules?
Thanks a lot!
Steven