Other Parts Discussed in Thread: ADS1232REF, ADS1232
Hi,
I have a ADS1232REF board and try to connect to a single-ended force sensor with internal amplifier. The output shows a drifting problem. The readout from the RS232 port drift down over time and it is so large that I cannot perform a calibration.
I also tried to connect a battery to the board and it also shows a drifting down problem.
For the connection: I connected In1- to GND as the data sheet suggested.
I did a shorted-input noise test. It did very well.
Then I tried to connect a load cell with internal bridge to the board, there is no drifting problem.
I am confused what is causing the drifting for single-ended connection.
Thanks!