This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mr Zengintas -
There are a couple of items to note:
1. Are you using the ADS1278EVM separate or with the motherboard?
The motherboard is required for power and connected signals unless you power the EVM board at the correct power terminals and provide necessary external signals.
2. The software is written to use the hardware with the default configuration. Changes from the default configuration will not allow the software to work or work correctly.
3. Using the EVM plugged onto the MMB0 may result in some contention between the DSP outputs and your signals. Make sure that the default state of the DSP pin is not overriding or causing contention with the signals you may be trying to provide.
Mr Gupp,
We are working on this project with Alper. The board isn't used with the MMB0 mother board. The EVM is connected to the Pandaboard. In addition, for once, I disconnected the DRDY pin from the Pandaboard in order to prevent complications and measured the DRDY pin with scope.
Kind regards,
Cumali Ceylan
Are you providing all the supplies to the board - AVDD, DVDD, and IOVDDD?