Other Parts Discussed in Thread: ADS5282
Hi,
I am intending to interface ADS5282 EVM with Altyera DE2-115 development board.
Referring to the DE2_115_User_manual_2013, page # 41;
Additionally, when LVDS is used as the I/O standard of the HSMC connector, the LVDS receivers need to assemble a 100 Ohm resistor between two input signals for each pairs.
I wonder if I have to assemble 100 Ohm resistor myself ? If yes, how ? Wouldn't it be difficult to add extra resistor to HSMC ?
Thanks.