Dear All,
I have modified the fifos in the fpga code in order to save some space on the fpga. The changes are:
fifo_96_4k ----> fifo_64_2k
fifo_48x16 ----> fifo_32x16
I would like to know what sort of changes are required in the script file (adc10d1000_xc4vlx25_adc08d1520rb.reg) in order to accommodate the changes in the fifo. I have found the part in the file that has to do with the acquisition part but it is uncertain as to what I am going to have to change.
I have the feeling that nothing can be done to fix this and that it has to do with stuff hard-coded in wv5, is this the case ? If this has to do with the firmware in the cypress, is it possible to have the code ? I have read somewhere in the forum that this is not possible, has the situation changed by any chance ?
Thanks in advance,
Evros