This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Stewart,
Sorry for the delayed response. When you see the high output, if you take a few captures, does the problem go away? How have you been fixing the issue?
As far as the unused inputs: The analog inputs on these devices are high-impedance so you should leave them floating if you are not using them.
The complementary DINs should both be tied low as per page 39 of the DDC11X product development kit which includes the DDC114 device http://www.ti.com/lit/ug/slau234a/slau234a.pdf
I have not seen the behavior you mentioned but maybe we can come up with a solution based on your answers.
Regards,
-Adam Sidelsky
Adam,
thank you for the reply - Your help with this is much appreciated.
We have found that the problem persists evens after a burst of ( >20 ) acquisitions. We have however found that the problem goes away if we reconfigure the Range setting on the DDC114, which is our current work around. For example, if we change from Range 0 to Range 1 and then back to Range 0, the problem goes away ( if the machine is left on for several hours, the problem might return )...
Please let me know if you need any more detail.
I look forward to hearing from you.
Kind Regards,
Stewart
Stewart,
Are you simply pulling the range 0 bit low and pulling the range 1 bit high? Are you sure that you are not resetting the device at all, changing the CLK speeds or CONV timing when this range selection is changing? In principle all that the range change does is disconnect the range 0 cap and then connect the range 1 cap, then reconnect the range 0 cap.
Regards,
-Adam
Adam,
in answer to your question, we start with :-
RANGE 2 is 0
RANGE 1 is 0
RANGE 0 is 1
then we change the following :-
RANGE 2 is 0 -> 0
RANGE 1 is 0 -> 1
RANGE 0 is 1 -> 0
and the fault clears.
We then set it back to :-
RANGE 2 is 0 -> 0
RANGE 1 is 1 -> 0
RANGE 0 is 0 -> 1
and the fault remains clear for some hours ( we have seen it return after > 4 hours ).
We do not change CLK speed or apply a (N)RESET and we do not change the acquisition timing.
Please let me know if you need any further information.
Kind Regards,
Stewart
Table 1. Range Selection of the DDC114
RANGE2 RANGE1 RANGE0 CF
(pF, typ)
INPUT RANGE
(pC, typ)
0 0 0 3 −0.048 to 12
0 0 1 12.5 –0.2 to 50
0 1 0 25 –0.4 to 100
0 1 1 37.5 –0.6 to 150
1 0 0 50 –0.8 to 200
1 0 1 62.5 –0.1 to 250
1 1 0 75 –1.2 to 300
1 1 1 87.5 –1.4 to 350
Stewart,
During your "idle" time (the few hours before you try bursting acquisitions again), what state are your CONV, CLK, VREF, and power pins?
Regards,
-Adam
Adam,
sorry, I've been tied up on another job.
As soon as I am able, I'll check the above and give you some feedback.
Thank you for following up on this question.
Kind Regards,
Stewart