why the wave shape of the red and IR is the same.
But according to this figure , the wave shape of the red and IR should be opposite. When wave of RED is on the crest, the wave of IR should be on the trough.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
why the wave shape of the red and IR is the same.
But according to this figure , the wave shape of the red and IR should be opposite. When wave of RED is on the crest, the wave of IR should be on the trough.
Hello Wei,
The first image below is the time series plot of the changes in light absorption also referred to as the photoplethysmogram (PPG). During each cardiac cycle, the heart is pumping blood to the periphery. The pressure pulse is detected by shining light with the LED (red and IR) onto the skin and then measuring the amount of light transmitted to a photodiode. Each cardiac cycle appears as a peak as seen in the image. Since it is the same cardiac cycle when Red and IR LEDs are alternately turned on, you will notice the same shape for both Red and IR phases.
The image below is the absorption coefficient of light at different wavelengths especially the red and IR wavelengths. The blue curve refers to the absorption coefficient at 0% SpO2 and the red curve refers to the absorption coefficient at 100% SpO2. This image provides insight into the wavelength dependent properties of blood. It shows that deoxygenated haemoglobin (HHb) absorbs more red light than IR light and oxygenated haemoglobin (O2Hb) absorbs more IR light than red light.