Other Parts Discussed in Thread: ADS1258
Hello ,
I have a problem with autoscan mode , I don’t understand when start the first channel in register mode.
Start when the START command is high or when send the first the register read command?
The reset , reset all the setting of the register?
If I read the first register 08h all is ok but when I read the entire register change the input channel position
Below my code :
Pic 32 mhz ads 8 mhz spi 500 khz
I have two converters connected in RC0 and RC7 CS ,now is one in RC7 only
/*programma bus isa
*/
#include <p18f97j60.h>
#include <stdio.h>
#include <stdlib.h>
#include <spi.h>
#include <delays.h>
#include <float.h>
void main (void)
{ int dato,rg1,sp,conta;
char dati[100],val,reg1,cbf[3];
long int pippo;
OpenSPI1(SPI_FOSC_64,MODE_00,SMPMID);
TRISB = 0X00;
ADCON0= 0X00 ;
ADCON1=0x00;
TRISC = 0x10;
PORTB = 0;
TRISE = 0XFF;
//dati[0]= 23;
//dati[1] = 10;
//dati[2] = 20;
//dati[3] = 30;
TRISD= 0X00;
conta = 0;
PSPCONbits.PSPMODE = 1;
//SSP1STAT = 0b00000000;// Configure register for SPI..(b6=0).
//SSP1CON1 = 0b00100010; // Configure register for SPI,
// scrittura dei registri del convertitore
PORTCbits.RC7= 0;
WriteSPI1(0b01100000);//comando scrittura registro0
Delay10TCYx(5);
WriteSPI1(0b00000000);//config0
Delay10TCYx(5);
WriteSPI1(0b01100001);//comando scrittura registro1
Delay10TCYx(5);
WriteSPI1(0b00000000);//config1
Delay10TCYx(5);
WriteSPI1(0b01100001);//comando scrittura registro2
Delay10TCYx(5);
WriteSPI1(0b00000000);//muxsch
Delay10TCYx(5);
WriteSPI1(0b01100011);//comando scrittura registro3
WriteSPI1(0b00000000);//muxdif
Delay10TCYx(5);
WriteSPI1(0b01100100);//comando scrittura registro4
Delay10TCYx(5);
WriteSPI1(0b11111111);//muxsg0
Delay10TCYx(5);
WriteSPI1(0b01100101);//comando scrittura registro5
Delay10TCYx(5);
WriteSPI1(0b11111111);//muxsg1
Delay10TCYx(5);
WriteSPI1(0b01100110);//comando scrittura registro6
Delay10TCYx(5);
WriteSPI1(0b00001100);//sysred
Delay10TCYx(5);
WriteSPI1(0b01100111);//comando scrittura registro7
Delay10TCYx(5);
WriteSPI1(0b11111111);//gpioc
//WriteSPI1(0b01101000);//comando scrittura registro8
Delay10TCYx(5);
//WriteSPI1(0b11001100);//gpiod
Delay10TCYx(5);
PORTCbits.RC0 = 1;
PORTCbits.RC6 = 1;
PORTCbits.RC2 = 1;
PORTCbits.RC7 = 1;
while (1)
{
reg1 = 0b00110000;
conta++;
LATD = dati[rg1];
switch (conta)
{
case 2 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[3] = ReadSPI1();
dati[4] = ReadSPI1();
dati[5] = ReadSPI1();
PORTCbits.RC7= 1;// cs
case 3 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[6] = ReadSPI1();
dati[7] = ReadSPI1();
dati[8] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 4 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[6] = ReadSPI1();
dati[7] = ReadSPI1();
dati[8] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 5 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[12] = ReadSPI1();
dati[13] = ReadSPI1();
dati[14] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 6 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[15] = ReadSPI1();
dati[16] = ReadSPI1();
dati[17] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 7:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[18] = ReadSPI1();
dati[19] = ReadSPI1();
dati[20] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 8 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[21] = ReadSPI1();
dati[22] = ReadSPI1();
dati[23] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 9 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[24] = ReadSPI1();
dati[25] = ReadSPI1();
dati[26] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 10 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[27] = ReadSPI1();
dati[28] = ReadSPI1();
dati[29] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 11:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[30] = ReadSPI1();
dati[31] = ReadSPI1();
dati[32] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 12:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[33] = ReadSPI1();
dati[34] = ReadSPI1();
dati[35] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 13:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[36] = ReadSPI1();
dati[37] = ReadSPI1();
dati[38] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 14 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[39] = ReadSPI1();
dati[40] = ReadSPI1();
dati[41] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 15 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[42] = ReadSPI1();
dati[43] = ReadSPI1();
dati[44] = ReadSPI1();
PORTCbits.RC0 = 1;// cs
case 16 :
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[45] = ReadSPI1();
dati[46] = ReadSPI1();
dati[47] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 17:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[48] = ReadSPI1();
dati[49] = ReadSPI1();
dati[50] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 18:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[51] = ReadSPI1();
dati[52] = ReadSPI1();
dati[53] = ReadSPI1();
PORTCbits.RC7 = 1;// cs
case 19:
PORTCbits.RC7 = 0;// cs
WriteSPI1(0b00110000);
dati[2] = ReadSPI1();
dati[54] = ReadSPI1();
dati[55] = ReadSPI1();
dati[56] = ReadSPI1();
PORTCbits.RC7= 1;// cs
case 20:
PORTCbits.RC6 = 0;
Delay10TCYx(1);
PORTCbits.RC6 = 1;
PORTCbits.RC7 = 1;
conta = 1;
}
PORTB = SSP1STAT;
if (PORTEbits.RE3 = 1)
{
if (PSPCONbits.IBF = 1)
{
dato =PORTD ;
PIR1bits.PSPIF = 0;
}
}
if (PORTEbits.RE4 = 1)
{
if (PSPCONbits.IBF = 1)
{
rg1 =PORTD;
PIR1bits.PSPIF = 0;
}
}
if (PSPCONbits.IBOV = 1)
{
PSPCONbits.IBOV = 0;
}
}
}
Regards
Bellotti Davide .