Hi!,
When I set the SELF_TEST of AFE5851, do I need to disconnect AFE5851's inputs?
Thanks in advance,
Toshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Toshi,
The Input channels to the AFE on the EVM are AC-coupled on the EVM. Therefore, the DC value applied at the input capacitor is isolated from the AFE input. Are you using the EVM?
Thanks,
Chuck smyth