Other Parts Discussed in Thread: OPA4350, LM741, ADS1251
Hi everybody !!! :)
I have a problem with rebuilding the signal in the computer, the Aliasing, so I need to find where is wrong, please just tell, if I've got a sample rate of 2400 KSP/S, then, I can acquire a 1KHZ signal whitout the aliasing is it not?-.
the data sheet says, prior the ADC, I have to use an OP AMP circuit to ensure the full scale. instead the OPA4350 I used the lm741 . is that the problem? to ensure a good acquisition do i have to use the OPA4350?.
Or the problem is Sofware.
ohh I forgot !! the adc is ads1251, in the oscillocope, I can see the data transmition to the microcontroller each falling egde.
thanks !!! so much have a good day!!