Hi,
We have a custom am335x board which is running linux3.2 and interfaced with ths8200. Our desired output format is vga 640x480@60. I set the register values according to the previous forum post -http://e2e.ti.com/support/data_converters/videoconverters/f/376/t/113249.aspx
FID pin is permanently tied to the ground, input signal is 16-bit RGB and RESETB signal is connected to WARMRSTn signal of SOC.
Finally signals are coming out but display is blank, anyone have any idea what might be the problem ?