What is the ads1256 input voltage range during system gain calibration? The ads1256 datasheet said
"System gain calibration can correct
inputs that are 80% of the full-scale input voltage and
larger. Make sure not to exceed the full-scale input voltage
when using system gain calibration."
Can the input voltage be a LARGER then 2*((Vref+)-(Vref-))?
For example in sbaa107 it is said
"This means that with the system GC, the ADC input range can be changed from 60% below to
33% above the nominal input range set by VREF/PGA." for d-s ADC of MSC12xx devices.
Practically my scheme based on ads1256 demonstrates the ability to perform system gain calibration with input voltage little larger than 2*((Vref+)-(Vref-)) (Vref=4,95; Vin=4,97) if it is not a mistake. And i'd know certain (or approximate) values if it is possible...
Thanks you for help.