This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DC coupled high speed ADC EVM

Other Parts Discussed in Thread: ADS4226, ADS4229, ADS4249, ADS4249EVM

Does TI have high speed ADC (>150 MSPS, >9 bit) EVM with DC coupled input? It will be great if it is possible to attach this EVM to TSW1405EVM.

  • Hi Konstantin,

    Please have a look at the dual channel ADS4249, ADS4229, ADS4226 which may meet your needs.  These also come in single channel ADS41xx.  Both are supported by the TSW1405.

    If you download the design package from the EVM product folder:

    http://www.ti.com/tool/ads4249evm

    you can see that there is an optional amplifier on the EVM (backside).  However you will need to do some mods to get it to work (remove/bypass the input transformer).

    Ken.