This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1258 unipolar use

Other Parts Discussed in Thread: ADS1258-EP, ADS1258

I have written this to support@ti but they put me to here. :)

I'm just wonder what are the differences between ADS1258 and ADS1258-EP. 

And the spec sheet indicated that it can use as unipolar operation, what is the full scale input range for the AD? Would it be 2xVref (0-5V)?

Thank you. 

  • Gary,

    The full scale input range of the ADS1258 is 1.06Vref. This information can be found on page 3 of the data sheet. If you are using a 2.5V reference, then your full scale input range would be 1.06*2.5V = 2.65V. This ADC can be run in unipolar or bipolar mode depending on the supplies and the configuration that you use.

    The ADS1258-EP is an enhanced part to the ADS1258 that is geared towards medical applications. The difference between the two parts is the ADS1258-EP has been rated and gauranteed across a larger temperature range (–55°C to 125°C) compared to the ADS1258 (–40°C to +105°C).

    Regards,

    Tony Calabria

  • My question was what is the full scale range for unipolar mode. All the specs on the data sheet are on bipolar mode. (AVdd: +2.5V, AVss: 0, FSR: +/-1.06Vref, FSR: -2.65 -> 2.65V with 2.5V Vref).

    I just want to know that the specs, to be precise, full scale range of the AD during unipolar mode (AVdd: +5V, AVss; 0). Would it shift to 2*1.06Vref (i.e. FSR: 0-> 5.3V with 2.5 Vref)? 

    And thank you for the info on the EP part. That is very useful. 

  • Gary,

    When the data sheet says that the part can be run in unipolar operation, it is refering to the power supplies. Setting the power supplies at AVdd = +5V, AVss = 0 will not have an effect on the input range. The input range would be 0 to 2.65 volts (+1.06*Vref) with a 2.5V reference.  Using a 5V reference the input range would be 0 to 5.1V because of the absolute input voltage range constraint that the input cannot be larger than AVDD + 100mV.

    Regards,

    Tony Calabria

  • Thank you Tony.