Other Parts Discussed in Thread: ADS1248
I'm looking into to use the ADS 1248 converter in one of my designs.
Have been reading the datasheet both forward and backwards, and there is a few things that I find unclear.
First of all, in the data sheet it says that that the number of singleended inputs is limited to 7, leving one input un-used., however can I use 2 say 1 differential and 6 single-ended inputs, totaling the number of inputs to 7.
Is the same limit applied if I use some of the inputs as GPIO's?
In my design I can't iuse the DRDY signal nor the START signal, Should I tie the START-input to DVDD and use the RDATA-command?
If I understand it correctly, when START is tied to DVDD it converts continiously, if so, how do I stop it in order to change channels and PGA settings etc.
Or is there another way to start the conversion, independantly of the START-pin? SYNC-command??