This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TVP5150AM1 XTAL/OSC Input clock

Other Parts Discussed in Thread: TVP5150AM1

Hi,

I'm using 4 x TVP5150AM1 in my design, and i want to use to OSC option instead of crystal (14.32 OSC => 1:4 clock driver => 4x TVP5150AM1).

1.Can i use 14.32MHz Clock instead of 14.31818-MHz?

2.What is the voltage level for the input OSC clock? (Figure3-8 in the TVP5150AM1 D.S shows TTL clock, while the absolute max rating figure is –0.5Vto 2.3V)

Thanks,Shahar.