This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
another inactive official forum. why official forums like this are inactive and has very few answers ?
I don't think that my question about this TI's product be very hard to answer for engineers in this forum. I bought this product and need to support for using it also there isn't sufficient resource and sample or typical circuit about this product in the web. Please help me to do my project with this product.
Thanks,
Regards.
Your schematic is correct. If the LCD you are using is a bit noisy, adding several decoupling capacitors, from Y+, Y–, X+, and X– to ground, is a good way to reduce the analog input noise from the LCD. For more information, you can take a look at the application note, which explains some very useful methods to reduce noise. Here is its link:http://www.ti.com/lit/an/sbaa155a/sbaa155a.pdf