Hi,
Whenever I connect Tx-SDK board and XEM3001 board the OTP led is turned high. This happens when there is no power supply connection given to the TX-SDK-V2 board and the FPGA is programmed with TX_EN and sLA as high. Is it happens usually? When I checked the +3.3 V supply rail it reads 2.45 V
I am afraid there is a short in the board.. Any information will be appreciated.
Regards,
Fathima
NET "FPGA_MODE" LOC = P119;NET "OTP_LED" LOC = P205;NET "FPGA_TX_EN" LOC = P148;NET "FPGA_ARST" LOC = P146;NET "FPGA_S_LA" LOC = P140;NET "FPGA_S_DATA" LOC = P138;NET "FPGA_S_CLK" LOC = P135;NET "FPGA_S_RD" LOC = P143;NET "SYS_RST_N" LOC = P194;NET "START" LOC = P191;NET "LOCKED_OUT" LOC = P204;NET "FPGA_PSR_EN" LOC = P132;NET "FPGA_SDI" LOC = P130;NET "FPGA_SCLKI" LOC = P114;NET "FPGA_SCSI" LOC = P126;NET "FPGA_SW_RST" LOC = P111;NET "FPGA_SPI_EN" LOC = P124;NET "FPGA_OTP" LOC = P116;NET "data<0>" LOC = P196;NET "data<1>" LOC = P197;NET "Y<0>" LOC = P203;NET "Y<1>" LOC = P200;NET "Y<2>" LOC = P199;NET "Y<3>" LOC = P198;
NET "hi_in<0>" LOC = "P79";NET "hi_in<1>" LOC = "P57";NET "hi_in<2>" LOC = "P58";NET "hi_in<3>" LOC = "P78";NET "hi_in<4>" LOC = "P61";NET "hi_in<5>" LOC = "P62";NET "hi_in<6>" LOC = "P63";NET "hi_in<7>" LOC = "P64";NET "hi_out<0>" LOC = "P81";NET "hi_out<1>" LOC = "P85";NET "hi_inout<0>" LOC = "P67";NET "hi_inout<1>" LOC = "P68";NET "hi_inout<2>" LOC = "P72";NET "hi_inout<3>" LOC = "P74";NET "hi_inout<4>" LOC = "P86";NET "hi_inout<5>" LOC = "P87";NET "hi_inout<6>" LOC = "P90";NET "hi_inout<7>" LOC = "P92";NET "hi_inout<8>" LOC = "P93";NET "hi_inout<9>" LOC = "P94";NET "hi_inout<10>" LOC = "P95";NET "hi_inout<11>" LOC = "P96";NET "hi_inout<12>" LOC = "P97";NET "hi_inout<13>" LOC = "P100";NET "hi_inout<14>" LOC = "P101";NET "hi_inout<15>" LOC = "P102";
NET "clk1" LOC = "P80";NET "SYS_CLK2" LOC = "P77";