Hello,
I just received an ADS42LB69EVM evaluation module which I hoped to be able to interface to my Xilinx KC705 FMC slot using the TI FMC-ADC-ADAPTER. Both use a SAMTEC Qstrip series connector (QSH on the adapter and QTH on the ADS board). Both are electrically pin compatible. However mechanically these two boards do note mate. The ADS board has two large pins on either side of the connector which appear to be used for mechanically supporting the connection. The Adapter board does not have a mating socket for these pins and consequently the pins interfere with bringing the boards together.
Upon taking a closer look at this document: http://www.ti.com/lit/ml/slab058/slab058.pdf it is clear that the ADS42LB69EVM is not supported by the adapter card. This is surprising and unfortunate since it seams to be so close to being compatible and because so many similar products are supported.
My question now are:
Is there a different adapter that will let me connect the ADS42LB69EVM to an FMC connector on my Xlinix KC705 board?
Is there an adapter to go between the two non-mating connectors?
Is it possible to replace the connector on either board with one which will mate?
For use in the lab is it possible to cut these interfering pins off using a dremel tool and mate the connectors?
Any suggestions or advice would be appreciated.
Craig