Other Parts Discussed in Thread: ADS1248, ADS1120, ADS1220
hello
We are using ADS1248 analog to digital converter in a two-wire RTD application. Our design is attached below. (Rbias=1K4 and RTD=1K). In this design, one channel is used as a negative input channel for the RTDs and five channels are used as a positive input channel for the RTDs so that five RTDs are measured in our design. On the other hand, the other two channel inputs are used for measuring an external signal.
In a room temperature, everything is fine and the conversion results are fine. However,while changing the ambient temperature between -40 C to +55 C , something goes wrong so that conversion results for the RTDs measurement became wrong but the other channel for measuring an external signal is still fine, there is no problem for it.
What may be the problem in our case? Current source of the ADS1248 seems corrupted in the our temperature tests, is it true? How can we solve this problem?
Best Regards,
Yavuz Delican