I am designing a data acquisition system where I need to capture differential analog signals that range from 0 to +-3.3 V (plus/minus) and having a common-mode voltage of +1.65 V. Resolution must be 24 bits and sampling rate must be at least 10-20 kS/s.
At first, under a quite long search, I chose ADS1274 24-bit ADC with 4 channels.I thought that having a reference voltage of 3.3 V would be enough.
However, on page 4 of the datasheet, it is stated that the maximum value of the reference voltage is 3.1 V. (fCLK will definitely be less than 27 MHz.)
Would it be safe to connect a 3.3 V voltage reference across the VREFP and VREFN pins of ADS1274 or should I consider another ADC? Can anyone give me a suggestion for this?