I'm having trouble with parallel configuration on the ADS62P49. I can do serial configuration, but in some application the number of control signals is limited and I need to use parallel configuration. Serial configuration works fine, but parallel configuration doesn't.
I have tied RESET high, SCLK low, and SEN to (5/8)AVDD. With CTRL1-3 pins I select MUX mode (111). Now all channel A works fine, channel B give strange results. Doing some experiments leans that the device seems to work corrent when RESET is tied low. I do not understand why, since the datasheet tells me RESET should be tied high (page 14).
Another strange behaviour related to the reset is the output format. When RESET is kept high, the output format is offset binary CMOS, but is should be 2's complements according to table 5 in the datasheet. But when RESET is tied low, the output format is 2's complement.
So I have two reasons to assume the reset should NOT be kept high for parallel configuration only, but I like to have a confirmation on this. I need to be sure if there is a risk not resetting the device.
Thanks,
Peter