Hello,
I am working with ADS1298ECGFE Rev C Board,
I'm trying to get SPI communication going.
However there seems to be a difference in the newest Documents with what is stated in this post http://e2e.ti.com/support/data_converters/precision_data_converters/f/73/t/105352.aspx?pi73718=2
Now it would be great if i could just blindly follow whats in the post above, where the person describes all the connections in detail.However some of the information is different like they mention the JP22 and JP27 open (internal oscillator), in the user guide JP27 is (2 Jumpers) WCT connected to CH7- input and ECG_V5 connected to CH7+ input
Can someone please give me some direction in hooking up the power and SPI, I would really appreciate it. Sorry if this is an already answered post, i might not have seen it.
My connections so far:
J4.5 = GND
J4.9 = 3.3V
J3.1 = CS
J3.14 = START
J3.15 = DRDY
J3.11 = DIN
J3.13 = DOUT