I want to make a datalogger to measure signals from -0.5Vdc to 0.5Vdc with a sampling rate of one minute, ie every minute obtain one sample, one-shot!
The battery that I will to use is 3.7Vdc and the ADC is ADS1282.
Should I put VREFN =- 2.5V, VREFP = 2.5V or less?? and Vin input connect directly with what is going to measure?
Or should I use a Fully Differential Amplifier THS4522 in ADC input? Or should I just use a passive filter?
What tensions do I have to put in VREFN, VREFP, AVDD and AVss? And which components should I use?
Regards,
Ivo Bernardo