Hello,
Does the clock input of the ADS1278 need to have a 50% duty cycle? Could I instead run it off a clock with a duty cycle of 1/3 or 2/3? For example, a clock that was high every one out of 3 cycles of a 80MHz clock for a clock rate of 26.67MHz.
Also, I am trying to generate the clock from a Tiva C Launchpad and would appreciate any comments you might have on the following post:
http://e2e.ti.com/support/microcontrollers/tiva_arm/f/908/t/324018.aspx
Regards,
Curtis Mayberry