Other Parts Discussed in Thread: AFE4490
Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE4490
Hi,
Hello Rob,
I apologize for the delayed reply.
1. The filter is a switched RC filter. Depending on the duty cycle, the bandwidth of the filter around DC gets scaled down from 500 Hz (lower the duty cycle, lower is the bandwidth). Also there are going to be copies of the primary frequency response (around DC) around every multiple of the PRF. Finally there is an envelope (close to a sinc function) whose width again depends on (inversely proportional to) the duty cycle. So overall, it is quite a complex function.
The details about the 22-bit del-sig converter is TI IP and will not be disclosed.
6. The 3-dB bandwidth of the TIA is determined by Rf and Cf and is equal to 1/(2.pi.Rf.Cf). The switched R-C filter follows the TIA and its bandwidth is not determined by Rf, Cf (refer response to Qn.1)
7. When you have a factor of 10, essentially you are giving 10 time constant for the TIA to settle to the pulse transients. It could be set to between 5-10.
8. Enabling averaging causes the ADC to convert the voltage sampled by the switched RC filter multiple times to reduce the ADC noise. The sampling is done once (across the capacitance of the switched R-C filter) and the same sampled voltage can be converted multiple times by the ADC (each conversion taking 50 us).
Best regards.