This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP is giving constant o/p

Other Parts Discussed in Thread: LMP90100

Dear Support team

This my config for LMP90100: VA = VIO = 4.5V , VREFP1 - VREFN1= 4V

VIN0=1V VIN1 = GND,  only single channel under use.  

address 0x20 = 0x01

address 0x21 = 0x31  //give SPS = 13   Gain = 2

address 0x1F =  0x08  // Last channel for conversion is VIN1

The ADC bytes I am getting are : 13 70 25 (all in Hex) for every  input voltage . ADC o/p is not changing.

I read back above registers and found OK.

Pls tell what went wrong.