Hello Mr.BOB. We have completed 1 product using ADS1147(input rtd or4-20mA) and it is working successfully. Now I am incorporating ADS1148 in another instrument where the field conditions are different. The input is thermocouple which is grounded and soldered directly to the target. The target’s temperature is to be measured. It is a heat treatment application where target’s temperature reading is to be monitored continuously for long periods. The reliability of the instrument is essential here. My input circuit schematic is as attached0250.CPU.pdf. Please refer sheet 2 and sheet 3 of the schematic where 2 ADS1148 ICs are used for 8 channel input. Can you suggest any changes in the input circuit so that the input circuit especially ADS1148 remains undamaged? Also is there any isolation required between ADS1148 and thermocouple?
Regards,
Dhiren