Other Parts Discussed in Thread: ADS1278
I have 2 questions regarding the ADS1278:
1) Is the sampling rate limited to the operating modes 144, 52, and 10 kSPS?
2) The datasheet states that "Fixing one of the inputs to 2.5V permits bipolar operation.." . If AINN is fixed to 2.5 volts can I apply a true bipolar input to AINP?
Thanks for the help.