Other Parts Discussed in Thread: ADS1294
Hello everyone, I need some help! Thank you ahead of time for the help!
I was using ADS1298ECGFE Rev C Board without the MMB0 with the following configuration to power it.
3.3V to TP10
GND to TP8
5.0V to TP7
It usually drew very little current on TP10 but when hooked up the power it drew up to .5A!
Im pretty sure that is not normal and I might have messed up my board. Now when I set it back with MMB0 it shows a weird number on the 7 segment display, and on the ADS129xECG-FE software it reads the registers really slow, and then shows an ID of a ADS1294!
Can someone please help me! Thank you