Other Parts Discussed in Thread: ADS7955
VA is 5V and Vref is set Range 2(2*Vref).
In this stage , input voltage range is 0V to 5V.
After this, the VA fell to 4.0V.
Thus, the input voltage range becomes 0V to 4V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ADS7955
Ryuji-san,
As per the ADS7955 datasheet, we spec the input range max as 2Vref with the condition that 2Vref <= VA.
The device can be used as you have described, with the input range restricted to VA+=4V. However, please note that you will not be able to get the full dynamic range of the device and the codes corresponding to the voltages between VA and 2Vref (in this case, 4V to 5V) would not be available.
NOTE: Care should always be taken that inputs should not exceed VA (=4V) else the ESD diode would turn on and distort the input signal.
Regards,
Sandeep