Hello,
I connected the EVM to the VC707 and solved the power problems.
But now I tried to configure the CDCE62005 on the board, but it doesn't work.
I have to use only the VC707 and this EVM. I tried the configuration with the "well" documented Labview program.
I can only use the onboard 19.2 MHz Oscillator. With the Configuration FB: 48, InputDivider: 1, Ref Divider: 1, Prescale 2 I got at the PLL_LOCK a 660 kHz signal with nearlly 60 % duty cycle.
In this configuration the Fvco is / should be 1843.2 MHz. but with output divider 10 I got a frequency of 84.4 MHz instead of 92.16 MHz.
If I use a higer number for R and I, so that the Fcomp will be lower I got no signal at the PLL_LOCK but nearly the same output frequency. Whicht is the right Value for Fcomp?
Using the 19.2 MHz as clock source works fine, but I need a clock configuration of nearly 400 MHz.
Can anybody help me?