Hi,
I will need change the firmware. Can I program the stratix IV (EP4SGX) using USB direct from Quartus II programmer? What changes do I need to do?
Could you provide me a CSV PIN ASSIGNMENTS?
Thanks
Danilo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I will need change the firmware. Can I program the stratix IV (EP4SGX) using USB direct from Quartus II programmer? What changes do I need to do?
Could you provide me a CSV PIN ASSIGNMENTS?
Thanks
Danilo
Danilo,
To be able to use the USB pod, you must install R55, R57, R58, R59, R60, and R129 and remove R61, R62, R63, R64. A CSV file is attached along with a .pin file, which is what I think you really wanted.
http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/68/6175.tsw1400_5F00_top.pin
Regards,
Jim
Well I'm just thinking, the HSDC uses usb to upload the firmware to FPGA. Why I need to change the board resistors? I'm starting to use this board, but I will need to use the CMOS connector and I'm making my own code to work with this board. Now I'm just want to make a simple led blinking work in this board and I would appreciate very much if somebody give me some tips to do it.
And don't know if the Pins Assignments that you send to me is what I need, or maybe I just dont know how to use it.
What can i do with '.PIN' file?
Thank you
Danilo