Hi,
As part of setting up the basic system for a project, I am trying to setup a hardware involving ADC - FPGA - DAC boards. For this purpose, I have a ADS54RF63EVM board, DAC34SH84EVM board, and Xilinx ML605 Virtex 6 board. I would like to interface these boards, and test by giving an input from function generator to the ADC board and observe output from DAC board on an oscilloscope.
1. After reading through lot of forum posts, I came to know that there are aspects such as setup time and hold time constraints that have to be taken care while interfacing the ADS54RF63 and ml605.
Is there any kind of source code or reference design I could look up at and learn, so as to do this interfacing ?
I had initially thought that I could collect the ADC output on the FPGA, create a FIFO module in the FPGA and then ouput it to the DAC board. Will it work that simple? Please help.
2. Any information on interfacing the ml605 with DAC34sh84 will also be of immense help.
Thanking in advance,
Basil Mohammed.