Other Parts Discussed in Thread: AFE4300
Hello everyone! We are interested in using the AFE4300 in an electrical bioimpedance measurement (IQ mode). But we want to be sure which is the frequency range of the chip and its accuracy. So, the question is: nowhere in the datasheet it is said what the maximum source signal frequency could be and the accuracy obtainable at this frequency. Using a 1 MHz external clock (as recommended), theoretically, the maximum attainable frequency would be 250 kHz (IQ driven directly by fclk, which should be 4 times the frequency of the DAC output, according to the sheet). Am I right? If so, anyone knows or has tested what is the accuracy measurement in those conditions?
Thank you all!