This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

230Vac sensing using AMC1100

Other Parts Discussed in Thread: AMC1100

I would like to design a voltage bus monitor for 230Vac, 50Hz. Variation expected on mains voltage is +/- 25% and negligible variation on frequency. I have referred the application report SLAA552 in which Fig 5. clearly shows the circuit for monitoring the instantaneous voltage. I require RMS voltage to be measured and not the  instantaneous voltage. It is also fine If I can get the peak voltage, so that RMS can be calculated. 

I have tried using bridge rectifier and a buffer capacitor between Line and R10 resistor in Fig 5. of application report SLAA552. But simulations are not convincing.

Please suggest circuit using AMC1100 to measure the input RMS.

Thanks and Regards

Senthil