Other Parts Discussed in Thread: DAC5688
Please let me know three points below about operation of DAC5688.
------------------------------------------------------------------------------------------------------
- Interpolation is used.
If it sees with a synchroscope from the input of data to an output, it will be delayed for about 4.4 μs.
Then, please let me know exact delay time.
(Is there any application note which calculates delay time?)
----------------
Specification of operation
CLK2=200MHz
NCO=50MHz
Interpolation=x4
----------------
- Does SNR change by the case where it does not use with the case where internal VCO is used?
(Is SNR improved if internal VCO is turned OFF?)
- While inputting fixed data into DAC and checking the output, whenever it reswitches on a power supply and does a setup of DAC again, the outputs of DAC differ.
if it is checking with the spectrum analyzer,an output with 3 patterns.
(What kind of output, its under a check)
Was there such any example in the past?
Specification is the following.
--------------------
20MHzInput
Sampling: 80x4Msps
Interpolation=x4
output: x2
--------------------
------------------------------------------------------------------------------------------------------
Thank you for your consideration.