Hi,
I've previously communicated with an engineer at TI that said the RESET line was not required on the ADS1298 and that the reset opcode could be used in place of the line, as indicated in the datasheet (p.34). We've built a system without the reset line because we were constrained on physical connections and tied the RESET line high. However, when we do this, we cannot connect to the ADS1298 over the SPI interface. It does not reset properly when sending the opcode for reset alone. We have confirmed this on the TI development board as well.
Can you please confirm if this is an error in the datasheet? Is the reset line actually required to properly reset the part after power on? Or is there some way the reset opcode can be used instead?
Thank you,
Jon