Hi every one,
In my project i am using ADS1291 24bit to read data .I am getting the data as shown below with CH1 and other one is power down mode. I am not getting 0xC00000 000000 when 0 input voltage applied at INP1P and INP1N.
For 0 input voltage, with internal reference 4.033V
C00000 FFF37C
C00000 FFF448
C00000 FFF445
C00000 FFF4E6
C00000 FFF487
C00000 FFF443
C00000 FFF33E
C00000 FFF41F
C00000 FFF430
C00000 FFF4A5
C00000 FFF4FB
C00000 FFF43E
C00000 FFF46C
C00000 FFF343
C00000 FFF41F
C00000 FFF466
C00000 FFF563
C00000 FFF45E
C00000 FFF45F
C00000 FFF381
C00000 FFF391
C00000 FFF41A
C00000 FFF464
C00000 FFF4F2
C00000 FFF444
so please suggest me what is the problem here???? Here i am reading with internal ref 4.033V, SPICLK 3.6 MHz, ADCCLK 2MHz , I am getting internal referrence 3.98V on VREFP Pin with respct to the AVss signal.
Power supplys using:
+/- 2.5V Analog and 3.3V DVdd and DGND. The schematic is shown below.
The other readings when input voltage is +1V ,
C00000 20 44 42
C00000 20 9C C4
C00000 20 68 DA
C00000 20 54 62
C00000 20 4C D0
C00000 20 4A 46
C00000 20 46 84
C00000 20 44 81
C00000 20 44 B0
C00000 20 47 BF
C00000 20 47 7D
C00000 20 46 41
C00000 20 45 18
C00000 20 45 55
C00000 20 46 6E
C00000 20 47 8D
When negative 1V appllied,
C00000 DF AB 67
C00000 DF AB 51
C00000 DF 55 30
C00000 DF 87 7B
C00000 DF 9D 3F
C00000 DF A6 1A
C00000 DF A9 8B
C00000 DF AA F4
C00000 DF AB A8
C00000 DF AB D7
C00000 DF AC 1B
C00000 DF AC 25
So i am requesting all please suggest me how to read the perfect values.
Thanks in advance
Regards
H NARASIMHA MURTHY,
Embedded Design Engineer.