Other Parts Discussed in Thread: ADS1274, THS4521, ADS1278
E2E,
We have been using the ADS1274 quite happily for some time now, but discovered a potential issue recently.
Our circuit is very similar to Figure 88 in the datasheet (sbas367F, revised Feb. 2011).
AVDD = 5V, DVDD = 1.8V, IOVDD = 3.3V, VREF = 2.5V, VCOM=2.5V
We are using the THS4521 to drive the analog inputs.
Normally our analog differential inputs range from approx. -2.5V to +2.5V, and we get stable ADC counts readings from 0 – 2^24, as expected. However, at times the output of the THS4521 could continue to rise up to its rail (nearly 5V). When the differential input to the ADC goes above +2.5V, to ADC count pegs to 0xFFFFFFF as expected, until the differential input reaches approximately +4.85V, at which time the ADC count values go berserk – seemingly random values from 0 – 0xFFFFFFFF.
From the spec, we understood that our differential input was allowed to go as high as AVDD + 0.1V (so 5.1V). Are we understanding this spec correctly? Or are we doing something that this part is not designed to handle?
Thanks for your help