This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VSP8133 CCD AFE : noise issue?

Other Parts Discussed in Thread: VSP8133

Hi

I have a issue.
Please give me a advice.

[Issue]
My customer is using VSP8133.
Rarely, it becomes a frame brighter than other frames since output pulse is floating.

[My reasoning]
I suppose that a coarse adjustment of the Black-Level clamping is performed at the head of the frame.
I suppose that when VSP8133 resived a noise from external at adjusting the Black-Level clamping,
it's occuered the above issue. 

[Question]
Q1:At which pin should the measure against a noise be taken?
   AVDD? or another? Please give me a advice.

Q2:Please suggest an example layout for the measure against a noise?
   The information on the product similar to VSP8133 is also available if it becomes helpful. 

Best regards
Shimizu