This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4300 clock generation

Other Parts Discussed in Thread: AFE4300

Hi! Finally we decided to build our own board based on AFE4300 in order to carry out bcm measurements (only module). However we have a doubt regarding its clock source: could a simple crystal oscillator of 1 MHz do the job or a specific chip like MAX7375 is needed? Since no information is provided in the datasheet, any suggestion about it? And another question: all the unused input pins should be connected to a gnd or vcc like usual fet inputs or can be left open? Regards