Other Parts Discussed in Thread: DAC38J84
Hi,
Our customer are considering their system as below.
・Center Frequency=2GHz
・bandwidth=24,32,56MHz
Please let me know if DAC38J84 could be generated these output frequency.
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DAC38J84
Hi,
Our customer are considering their system as below.
・Center Frequency=2GHz
・bandwidth=24,32,56MHz
Please let me know if DAC38J84 could be generated these output frequency.
Best Regards,
Kato
Hi Kato,
In order to output a signal at 2 GHz, the image in the 2nd Nyquist zone would have to be used. The DAC38J84 is designed to be a 1st Nyquist zone DAC, but a signal could be output in the second Nyquist zone. The issue is that the sine(x)/x response of the DAC will attenuate the signal and thus limit the performance. So the simple answer is that yes, the DAC can output this frequency, however the performance will be degraded due to the attenuation of the signal.
Regards,
Matt Guibord
Matt -san,
Thank your for the reply.
I have additional questions.
Please let me know how much the signal would be attenuated at 2GHz.
And what is the output frequency from 1.5GHz to 2.5GHz to get the best performance?
Best Regards,
Kato
Hi Kato-san,
Are you referring to the sampling rate or the output frequency? Generally you'll want to avoid HD2 and HD3. If the center frequency is flexible, then lower is better. The avoid HD2 and HD3 while running at 2.5 GSPS, the center frequency should be kept below 1600 MHz. There may be clock mixing spurs that should be avoided as well.
To output a signal in the 2nd Nyquist zone, a signal in the first Nyquist zone should be created such that Fs - Fsig is the desired frequency. For instance, to output 2 GHz while running at 2.5 GSPS, you should generate a signal at 500 MHz.
Regards,
Matt Guibord