Other Parts Discussed in Thread: DAC8814
Hi
Although DAC8814 datasheet describe VOH (min) is 4V, Is it applied VDD is 3.3V?
If it is not , what value is VOH when VDD is 3.3V?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The DAC8814 can be supplied with VDD ranging from 2.7 to 5.5V. The datasheet specifies the VOH (min) as 4V, which is a typo. The value of VOH depends on the supplied VDD voltage. The DAC8814 has a CMOS input and in your case with VDD of 3.3v, the VOH (min) should be about (3.3 - 0.7) 2.6V. Also keep in mind this VOH (min) is specified at 100µA current load.
Regards,
Neeraj Gill