Hi
I am a user of ADS1256. Now I have some problems in its PGA setting. Here is the phenomenon. I use the differential input mode, and I attach AINn to AIN0 and AGND, AINp to AIN1 and 40mv. When the PGA =1,2,4,8,16, the outputs were right, but when the PGA=32 or 64 the outputs are 76mv and 1050mv not 1280mv and 2560mv. And this time the noise was very large. I cannot find the reason please help me, think you!