This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stand-Alone ADS8411 or Equivalent ADC Circuit Without a Microprocessor



I am trying to build a circuit using an Analog-to-Digital Converter (ADC) as a stand-alone converter with no microprocessor. I need parallel output as I am using some of the LSB's to convert into an Incremental Encoder using XOR gates. This is for a Linear Actuator project using a Linear Potentiometer. I would like to use at least a 12-bit ADC or higher. Does anyone have a quick, easy interface circuit to drive the conversion on the chip? Thank You.